AVAC Vakuumteknik CEA Vacuum Gripper
Avac CEA foam gripper can handle a wide variation of objects with ease. The vacuum gripper provides an extra secure function with a preventive maintenance signal. The unit can indicate when it’s time to change the foam rubber before it wears out and loses the ability to grip. A modular standard system makes it possible to tailor the suction power according to the demand and also build custom made vacuum end of arm tooling / vacuum cups. There are different means of releasing the object to make sure it is released in a safe and secure way. Using standardized components, the CEA Vacuum gripper represents a great value at a competitive price point.