Leverage Robotics ToolCube Box
The Leverage Robotics ToolCubes are automatic exchangeable robot tools to perform multiple tasks on one robot. They expand the possibilities of a simple two-finger gripper by a multitude of options like vacuum gripping, centered gripping of round objects, or magnetic gripping of ferro magnetic objects and still keeping the capabilities of the parallel gripper.They can be used with a standard robot gripper and are purely passive: a voltage supply or vacuum generation etc. is not necessary. Only the existing gripper jaws have to be exchanged for the enclosed gripper jaws. The tools can be placed and used anywhere in the work area, thus avoiding unnecessary long travel distances and reducing cycle times. The ToolCubes use minimize set-up times and significantly increase the flexibility of the robot system.