Ultraflex Solo Dragon 24
The Solo Dragon 24 integrates the 24kW SOLO Series induction heating system with a Universal Robot (UR5, UR5e, UR10, UR10e, UR16e) to achieve a fully automated brazing process. The induction heating system has been successfully used to replace the outdated and unsafe torch brazing widely used in the industry. The integrated induction coil mounted directly onto the robotic arm is capable of reliably brazing multiple joints by applying controllable heat precisely positioned by the robotic arm.